4/8/2019 2:15 PM | |
Joined: 9/16/2016 Last visit: 3/22/2024 Posts: 3 Rating: (0) |
I am also having problems with this. I want to send e-mail via message window as an alarm triggered by tag change. In email-configuration settings I have set the following: e-mail server address: smtp.gmail.com I have founded also on Siemens forum Google internet authority certificate G3 that is valid till 12/15/2021 that should allegedly allow me the SSL e-mail transfer. I have imported it also under security/certificate manager section of my CP1242-7 module, but I always get the same error message number hex 8420- "Certificate chain from the server could not be verified with the root certificate of the CP." Why this certificate isn't valid? Where can I import other certificates because I cant' see to find them on internet? Is there anything else i should/must change in my settings? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/9/2019 9:32:20 AMNew subject after splitting |
|
Follow us on