4/8/2009 8:34 AM | |
Posts: 2 Rating: (1) |
2. Hardware details with MLFB nos. AttachmentPraj-PLC Hardware BOM.pdf (1830 Downloads) |
4/8/2009 12:11 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello khushal; |
This contribution was helpful to2 thankful Users |
10/27/2016 10:40 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, this would be the best for beginning: CPU-CPU Communication with SIMATIC ControllersYou will find every possible way to communicate between two Simatic PLC. For detailed Information of the communication you coose, you can search the search window on the upper right on this page. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to2 thankful Users |
10/28/2016 9:16 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, I guess you have two S7-400 DP-CPU´s. At least I understand so. Have a look to page 138 of the suggested manual, see attachment. for communication with both PLC as master, you need to establish aS7-connection and use the blocks"USEND/URCV"or "BSEND/BRCV"or "PUT, GET" A FAQ with application sample for using the instructions PUT/GET you will find here: What are the differences between the PUT and GET instructions for S7 communication and S7 basic communication?
If you decide to use other blocks, I recommend you to use the SEARCH BOX on the upper right. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to2 thankful Users |
6/26/2017 5:48 PM | |
Joined: 5/8/2017 Last visit: 6/27/2024 Posts: 14 Rating: (0) |
yeah Hi, Can you help me to communicate with two different PLC i.e. S200 and S300. over TCP/IP. |
6/26/2017 6:50 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello ajrj; Must it necessarily be through TCP/IP? it would be simpler to use Industrial Ethernet, between the CP 243-1 (for the S7-200) and the CP 343-1 (on the S7-300 rack). Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on