6/10/2009 2:27 PM | |
Posts: 163 Rating: (0) |
Thanku all.For communication between two nos. of H stations,my configuration goes link this am i correct? And im planning to follow this link https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=18513371&caller=view There are two H stations in my project which has communicate with each other. Attachmentnetpro.zip (223 Downloads) |
Last edited by: CS Moderator at: 6/10/2009 8:11 PMnew subject after splitting |
|
6/11/2009 6:05 AM | |
Posts: 163 Rating: (0) |
Ok I will try with S7 fault tolerant connection and my configuration goes like this.Tell me is it correct? Attachmentnetpro.zip (213 Downloads) |
6/11/2009 11:07 AM | |
Posts: 557 Rating: (64) |
HI check your attachment,it is still showing a TCP CONNECTION. PLEASE CHECK THE ATTACHMENT........... REGARDS Attachmentuntitled.zip (205 Downloads) |
Last edited by: Eastern at: 6/11/2009 11:16 AM |
|
6/11/2009 11:46 AM | |
Posts: 163 Rating: (0) |
I tried with S7 fault tolerant connection,got some errors. Why both my H Stations should be under the same project?is it because it has communicate with each other or for establishing s7 connection between them or is it possible to communicate even if i develop both projects seperately Attachmentnetpro.zip (197 Downloads) |
6/11/2009 12:59 PM | |
Posts: 557 Rating: (64) |
HI Please find the attachment... For software programming you can use GET(SFB14), PUT(SFB15) regards Attachmentuntitled.zip (210 Downloads) |
Last edited by: Eastern at: 6/11/2009 1:01 PM |
|
This contribution was helpful to1 thankful Users |
6/12/2009 9:01 AM | |
Posts: 163 Rating: (0) |
I don get errors when i connect the two H stations through s7 connection whereas s7 fault tolerant connection gives me some errors.Pls find attached. Attachments7 connection1.zip (243 Downloads) |
Follow us on