7/14/2020 10:27 AM | |
Joined: 6/16/2016 Last visit: 5/17/2022 Posts: 4 Rating: (0) |
Good afternoon, I need your help. There are two virtual machines on the PC, the scada is installed on the first, the simulator is installed on the second, PLCSIM advanced 2.0, with the project, you need to make a connection so that there is a connection between the scada, simulators, and the peripheral controller. in the application structure. In a virtual machine with a simulator, ping is a simulator, but there is no ping from the main operating system. Virtual Machine 1 (Windows 7). Virtual Machine 2 (Windows 7), Host (Windows 10)
AttachmentПрезентация1.pdf (74 Downloads) |
Last edited by: Jen_Moderator at: 07/14/2020 12:11:26Edited text for better reading. |
|
8/11/2020 3:50 PM | |
Joined: 8/3/2009 Last visit: 5/10/2024 Posts: 12924 Rating: (1646) |
Hello noface86 If you cannot perform a Ping the its a matter of Network settings in Windows. If you cannot connect the HMI SCada to the PLC or Simulation but the Ping is OK then you have to check the PGPC interface settings or project settings. Check this FAQ: https://support.industry.siemens.com/cs/de/en/view/109748099 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on