11/11/2019 11:16 PM | |
Joined: 9/27/2006 Last visit: 3/28/2024 Posts: 12249 Rating: (2660) |
Hello Stoked; I would suggest you use Get/Put instructions (for S7 Communications), these only need to be setup on one of the CPUs, over unspecified partners. The amount of data tranfered is relatively small, but you only need to configure the connection and the functions on one of the CPUs, the client; the other acts as a passive server. See the following documents: Read out information on PUT/GET instructions in chapter 7 of this manual, especially the section "Configuring S7 connections for PUT/GET instructions": https://public.eandm.com/Public_Docs/s71500_communication_function_manual_en-US_en-US.pdf Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on