8/17/2015 2:10 PM | |
Posts: 7 Rating: (0) |
Hello I am trying to establish a connection with PC,PG and PLC via Teamviewer VPN connection. But i didnot do it. i cannot ping PLC. IP address of PLC: 192.168.0.10 and router address : 192.168.0.9. I have tried step by step, again and again for 4 days. But it did not it.Could you help me about it ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/17/2015 3:35:12 PMNew subject after splitting |
|
8/17/2015 3:59 PM | |
Posts: 7 Rating: (0) |
I have changed Ip address of plc (i did it 192.168.1.10) and now i can ping PLC from local PC. But i can not see the plc in the accessible devices in TIA Portal |
3/31/2016 6:03 AM | |
Joined: 8/26/2014 Last visit: 2/23/2023 Posts: 14 Rating: (1) |
Hi all, I had tried the connection via teamviewer vpn according to the attachment. I can ping PLC from remote PC however when i come to get online via TIA portal , it failed to established the connection. I am no idea that what is the problem that caused this as i can ping the PLC. Is there any other method to troubleshoot this issue? AttachmentHow to setup Teamviewer VPN.pdf (1621 Downloads) |
Last edited by: loops0901 at: 3/31/2016 6:06:40 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on