10/25/2006 9:11 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hi, When you want to use a CP441-2 you have to use the Bsend and Brcv. You als must have the Modbus software ptp, including a dongle. When you install the software, there is also an example installed in Step7. Open project and look in tab Sample projects. Here you can download PtP software Modbus master: http://support.automation.siemens.com/WW/view/en/8713784 And here if you want to use Modbus Slave: http://support.automation.siemens.com/WW/view/en/8715908 Hope this will help. Best regards, Wizard |
Follow us on