7/22/2013 9:04 AM | |
Posts: 1064 Rating: (72) |
that depends on how much data and is time critical? |
7/22/2013 9:22 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Krsh, How much data you have to exchange? |
7/22/2013 12:59 PM | |
Posts: 59 Rating: (1) |
Hello Ayman, Please note that i am not using MPI network. Thank you. |
7/24/2013 10:39 AM | |
Posts: 1547 Rating: (129)
|
Hi Krsh, ok it is a standard configuration. You have to use an ISOonTCP connection. Create on each station three connections to the other stations. Create for example for each station a DB where the data of the station should be located. Use the functions FC5 and FC6 to transfer the data between the stations. The maximum amount of data per Job can be up 8 kByte. I think this should be enough. A detailed description how a Send Receive job works you will find in the NCM manual in Step7 Documentation folder in Start menu. A detailed sample how to call the FC5 and FC6 you will find here: How do you program the communication blocks FC5 and FC6? |
This contribution was helpful to1 thankful Users |
7/24/2013 10:50 AM | |
Posts: 1064 Rating: (72) |
Yopu could also use tcp ip instead of iso if you prefer |
Follow us on