4/22/2020 9:23 AM | |
Joined: 7/20/2016 Last visit: 3/29/2023 Posts: 1 Rating: (0) |
Hi, May I ask if the FO profibus cable and standard copper cable are using the same profibus ports? With the existing Profibus DP expansion module for PAC meters, is the customer able to install FO profiibus cables? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/22/2020 10:23:57New subject after splitting |
|
4/22/2020 12:58 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello; The screenshot below shows how to connect Profibus nodes to a fiber-optic cable. Each node connects over copper cable to an OLM (optical link module), the PLM connect between the with fiber-optic cable in various topologies. The image shows the OLMs in a ring topology. In the case of your project, you would need 2 OLMs in a simple line topology. The manual below explains the differences between OLMs, depending on the type of fiber (G=glass or P=plastic), the distances you need to cover, and the number of f.o. ports: - OLM P11 uses plastic fiber, for connections of 80 or 400 m , depending on the type of plastic cable; it has one copper port, and one f.o. ST port. - OLM G12 uses glass fiber, for longer distances ( you still have to decide whether you want multimode or single mode fiber, and what frequency optical signal you will use) and has 2 f.o. ports ( for star or ring topologies).and 1 copper port. You will find all the details in this manual on OLMs: https://support.industry.siemens.com/cs/ww/en/view/24164176 If you need more help after studying the manual, din't hesitate to come back and ask. Hope this helps, |
Last edited by: dchartier at: 04/22/2020 16:57:10Last edited by: dchartier at: 04/22/2020 17:06:26 |
|
Follow us on