11/22/2016 5:59 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, you have some antivirus enabled? I found this thread is not the same OS but if you want to read: step7 cannot load the selected communication driver:file not found ... |
11/22/2016 6:18 PM | |
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello, 1-Try to deactivate:antivirus and firewall program. If the problem not solved:try.... 2-Remove completly Step 7 then re-install it again according to the following FAQ: How do you uninstall STEP 7 completely, including all the software packages? |
Eng.Mohamed Ibrahim |
|
11/22/2016 6:22 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
OFF TOPIC, Dear Mohamed, wow finally Gold go ahead to reach Platin |
This contribution was helpful to2 thankful Users |
11/26/2016 2:50 PM | |
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello,
Perhaps the following FAQ might help: Menu item "Set PG/PC interface" missing in the SIMATIC Manager |
Eng.Mohamed Ibrahim |
|
11/26/2016 3:32 PM | |
Joined: 2/23/2016 Last visit: 7/1/2024 Posts: 12 Rating: (1) |
it deosn't work my freind thank you |
11/26/2016 8:02 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Have you already seen this in particular first post of Christoph: and |
This contribution was helpful to1 thankful Users |
11/29/2016 10:12 AM | |
Joined: 2/23/2016 Last visit: 7/1/2024 Posts: 12 Rating: (1) |
I saw it but it doesn’t also I became crazy with this problem thkx for your answer |
11/29/2016 10:32 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Hello, sry, what problem you still have? I had problem with my Ethernet card driver long time ago, had uninstalled it and installed older (before version), that solved my problem. With not showed interfaces/options on PG/PC interface in Win7 x64, that attached bat file helps me everytime. Look for first to internal of file what makes, check if path is same, run that bat as Admin (as it can run as) and wait to end, or run by your own like is inside of file with that parameter. Very same system show also Christoph, never used that but this. Hope this solve your problem. AttachmentPG_Interfaces.zip (219 Downloads) |
With best regards... |
|
This contribution was helpful to1 thankful Users |
Follow us on