9/14/2019 3:55 AM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
Dear Junaid , which PCS 7 Software version are you using right now? Which software package are you installing? Which Window Version (FullName) are you using? with these three pieces of information, I will compare it with Compatibility Tool |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
9/14/2019 6:39 PM | |
Posts: 10 Rating: (0) |
I am using PCS 7 Ver 9 and I am installing engineering package. I use win 7 ultimate Sp1. Regards Junaid Atta |
9/15/2019 4:41 AM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
Dear Junaid, Your window and version is okay. I never faced this kind of problem before. Is this is clean installation without any other Siemens Related software installed before? A clean installation is always recommended which means no other Siemens Software installed on the window before. Few suggestions here, hope it helps. 1. Try to get other stations, install the software again. 2. Try to use Window 7 Professional instead of Ultimate, or any other approved window. 3. Try to proceed the installation, then reinstall again with only WinCC click. Select User-defined installation. 4. Try to install with the Siemens CD, not to use ISO file. Following links are for your extra information. An Error Occured while installing the pcs dll Fail to communicate with server Hope it helps you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on