6/25/2020 5:20 PM | |
Joined: 11/12/2019 Last visit: 8/3/2021 Posts: 2 Rating: (0) |
Were you able to solve this problem? I am having the same issue. Details: I can download to the PLC but when I try to flash the PLC I get the same error message. In addition if I scan for devices on the Ethernet card I do not get any results so I had to manually enter the ip address of the PLC. I was able to do these things fine with an older borrowed computer running windows 10, but I need to get this working on my computer. I cannot connect to my HMI even using the IP address, (I can ping it fine). When I used Proneta to look for it, it showed up briefly and then disappeared. I have tried disabling the built in firewall and antivirus with no effect. I am running tia v16, windows 10 pro connected directly to the plc. I have tried dongles and switches with the same results. ------------------------------------------------------------------------------------------ |
Last edited by: BiogreenIan at: 06/25/2020 17:49:51Last edited by: BiogreenIan at: 06/25/2020 18:14:34Last edited by: Jen_Moderator at: 07/02/2020 09:30:18New subject after splitting |
|
7/2/2020 9:31 AM | |
Joined: 6/19/2017 Last visit: 5/7/2024 Posts: 8002 Rating: (163) |
Closed cause question posted twice. The second thread with the subject Flash LED function not working (among other things) is published within the conference Communication / Networks. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on