12/27/2019 7:43 AM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating: (15) |
Hi, it sounds like a little nasty issue you are facing ... I guess it could be a EMC related issue. I am not an expert in this field but what I can say is, double check the earthing and the electromagnetic shielding everywhere. Check if the shield of the Profibus cable is mounted proberly in all connectors and check if the earthing itself at each remote station is ok. |
iba AG - Data Acquisition and Analysis the way it should be |
|
Follow us on