3/9/2017 8:56 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
Absolutely agree... |
With best regards... |
|
This contribution was helpful to1 thankful Users |
3/28/2017 2:26 PM | |
Posts: 3093 Rating: (322) |
Back to the feedback for FAQs. In the meantime I sent the third feedback to update this FAQ for CPU410. At least half of the necessary information is available, the rest is still missing. If Siemens doesn't want feedback, they should keep FAQs update and delete the feedback button. Even the Mods could not give a statement here.... Regards, |
Last edited by: Kaulquappe at: 3/29/2017 10:48:38 AMAddendum: my third feedback caused a reaction/correction within two hours. |
|
3/30/2017 1:00 PM | |
Joined: 9/1/2005 Last visit: 5/10/2024 Posts: 4100 Rating: (193) |
Dear User, let me start with a quote
Maybe this is one reason why moderators weren't active in this thread earlier. We were in contact with a few different persons which are addressee of feedback messages. The messages they receive via the feedback channel are very different. But it seems that there are a lot of questions about assistance that are forwarded via the feedback functionality. Maybe we will need a more transparent functionality in the future to give you the chance to do both give feedback or ask for details when you are checking one of the existing documents.
We have checked the history of this FAQ. Why this update takes so much time, ... I don't know. But your tenacity takes effort. Please do not stop to provide your opinion on the published documents. But be a little bit patient if it takes a longer time until the feedback is verified or if you didn't receive the reply you are looking for. There could be a lot of reasons for that. If we could be for assistance to clarify specific cases please feel free to involve us moderators in the discussion. Best regards |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to5 thankful Users |
4/11/2017 11:29 AM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190) |
"Back to the feedback for FAQs. In the meantime I sent the third feedback to update this FAQfor CPU410. At least half of the necessary information is available, the rest is still missing." @Kaulquappe: The mentioned FAQ was updated on 28.03.2017. Do you find all your feedback in it or do you something missing, which you have send via the feedback form? |
SIMATIC PCS 7 - Overview |
|
Follow us on