3/10/2020 7:52 AM | |
Posts: 16 Rating: (0) |
I need GSD file for 6FC5373-0AA30-0AB0 ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/10/2020 08:38:00New subject after splitting |
|
3/10/2020 7:59 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hi, for what you need this?
Christoph |
3/10/2020 8:21 AM | |
Posts: 16 Rating: (0) |
If you create a PLC network with Eplan, You can export it into AML format, By importing this AML file in TIA you will get complete network as in EPLAN with all PLC Devices with Bus data, Addresses and Tag lists AML file uses some Identifiers like MLFB number & Ident number from GSD/GSDML file to identify the device in attachment you can see how AML file define Identifiers by using them TIA and EPLAN identify the Devices to import and export Attachment2020-03-10 08_06_49-KO_EL_EPLAN_Eplan_Prj2_Auto_Plan_1_Projects_9_Akshay_Projects_AutomationML.png (77 Downloads) |
3/10/2020 8:45 AM | |
Posts: 16 Rating: (0) |
Yes it work same for the Non-Siemens Devices Like Beckhoff I defined some identifier from GSDML file of Beckhoff & I got the result, But with SINUMERIK NCU I'm not able to match these identifiers AttachmentKO_EL_EPLAN_Eplan_Prj2_Auto_Plan_1_Projects_9_Akshay_Projects_AutomationML.png (52 Downloads) |
3/10/2020 9:01 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, because the SINUMERIK NCU is not modeled with GSD/GSDML in TIA Portal. Is a integrated component which is installed with the Toolbox. So there are no GSD/GSDML syntax or something like that available for the NCU. you can try to open a support request and ask if the Import/Export is supported for the SINUMERIK Device.
Christoph |
3/10/2020 9:08 AM | |
Posts: 16 Rating: (0) |
Thank You |
3/10/2020 9:12 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
can you provide the AML file you use for the NCU? Regards Christoph |
3/10/2020 9:48 AM | |
Posts: 16 Rating: (0) |
the data in AML file will change as I change it in Eplan device properties while Exporting it. I'm trying with multiple identifiers but its not working |
Follow us on