1/9/2020 10:25 AM | |
Joined: 6/5/2018 Last visit: 3/29/2024 Posts: 44 Rating: (0) |
hi profs im using this config: HW : S7-1200 1212 DC/DC/RLY + CM1241 RS232+Other modules shown in atach file SW:TIA Portal v15.1 v4 latest updates i want to send and receive data sample like word memory (mw2 = 1) to PC With ptp communication i using hercules v 3.2.8 , serial port terminal v1.0.0.0.710 and modbus poll programs on PC im not any errors in my programs block (PORT_CFG & SEND_PTP & RCV_PTP): PORT_CFG : REQ = CLOCK 1HZ PORT = 273 'Local ~ CM_1241_(RS232)_1' BAUD = 6 (9600) PARITY (none) = DATA BIT (8) = STOP BIT (1) = FLOW CTRL (none) = 1 XONCHAR = XOFFCHAR = " " WAIT TIME = 2000 STATUS = 7000 ERROR = DONE = FALSE SEND_PTP: REQ = CLOCK 1HZ PORT = 273 'Local ~ CM_1241_(RS232)_1' BUFFER = MW2 (initial Value = 16#0001) LENGTH = 2 PTRCL = FALSE STATUS = 16 # 7000 and sometimes 7002 ERROR = DONE = FALSE RCV_PTP: REQ = CLOCK 1HZ PORT = 273 'Local ~ CM_1241_(RS232)_1' BUFFER = MW4 (Initial Value = 16#0000) STATUS = 16 # 0000 ERROR = DONE = FALSE Control panel > device manager > COM Port > COM2 (9600,8,none,1) i attach a zip file and this video address (copy in our browser to download ) : http://uupload.ir/filelink/5DDJSCwAA2wl/amaj_record_2020_01_09_11_52_04_432(1).avi can anyone help me or send a useful link for solve ? thx AttachmentDesktop.zip (63 Downloads) |
Last edited by: Automation+ at: 01/09/2020 10:43:09Last edited by: Automation+ at: 01/09/2020 10:43:51 |
|
1/9/2020 11:57 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818)
|
Hello, in my side all work. |
With best regards... |
|
Follow us on