4/29/2020 5:11 AM | |
Joined: 1/4/2013 Last visit: 9/16/2024 Posts: 72 Rating: (2) |
I need help from anyone with access to run a test on a 414H, 416H or 417H PLC system. The purpose of the test is to measure the communication performance and compare with the 412H system that we have. The test works by sending UDP datagrams from one rack to the other and measures the time this takes. The complete test should take less than 10 minutes. The test program is attached, and the test procedure is as follows:
The test results “Test_4byte”, “Test_1472byte” and “Test_Execution” should differ by less than 2% from sample to sample. Save a screenshot of the stored actual values in the offline DB10. AttachmentCPU_UDP_test.zip (48 Downloads) |
Follow us on