11/20/2013 7:08 AM | |
Posts: 461 Rating: (29) |
U can do this configuration in the Harware config of the plc Create 2 plc's in device view & connect them thorugh profinet in the network view.. Perform download.. This links provide u the types & ways for communicating 1200 & 300..Select the ttype of communcation ur gonna use ,open or tcp ..U can find sample programs for both here Regards, Nelliyan.G |
This contribution was helpful to1 thankful Users |
1/22/2016 12:50 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
New question published by Mateus is split to a separate thread with the subject Examples of communication in L-COM by PROFINET between S7-300/400 and S7-1200. Best regards |
1/22/2016 11:51 PM | |
Joined: 2/18/2015 Last visit: 1/16/2024 Posts: 66 Rating: (5) |
Hello, This manual can be helpful. I've just validated it. Attachments7communication_s7-1200_s7-300_en.pdf (3076 Downloads) |
This contribution was helpful to3 thankful Users |
11/10/2016 9:44 AM | |
Joined: 8/21/2014 Last visit: 4/23/2024 Posts: 951 Rating: (13) |
New question published by jhing is split to a separate thread with the subject Connection between S7-300 und S7-1200 with TIA V13 possible?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on