12/12/2019 11:18 AM | |
Joined: 7/25/2011 Last visit: 4/17/2024 Posts: 20 Rating: (0) |
Hello! I am working on a project where I need to communicate with a underwater GPS system. To communicate they have a HTTP API command system. I need to send a HTTP API command, and then I get information back. I wonder if it is possible to do scripting in WinCC advanced to communicate with HTTP API or if it is possible to do this from a PLC, S7-1200. I need to sent a Get API en the I need to store the answere in a variable. Information about communication is here on theyr demo page: http://demo.waterlinked.com/swagger/ In attached picture you also see data for Get position. If I understand correct I need to send API global command to IP adress for GPS, then I get the position back. I would be very happy if someone know anything about this issue and can help me with information about where to start. I have already asked in the TIA Portal, but I think this is the right place. Best regards Andreas |
12/13/2019 7:29 AM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7959 Rating: (162) |
Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on