9/7/2019 10:40 AM | |
Joined: 8/25/2019 Last visit: 1/22/2024 Posts: 4 Rating: (0) |
Dear Sir I am using Matsterdrive mc compact plus and Chasis units for sheet cutter application, we parameterized with 368=3 ,On command via DI-X101-8-P554=20speed set point via MOPX101- DI6-P573=14 &X101- DI7-P574=16 for speed raise and lower and main set point connector KK0058 Aalso put in P443, first time drive was started and speed also increased/decreased,we restarted the drive second time drive is ON but speed is not increased and decreased but inputs are coming and checked with r550 is ok and speed set point is not coming at r424 when push the buttons of raise and lower,please and PMU is flashing 1 and -0 continuously give me solution to run the system Thanks & Regards S.Thangamani
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/09/2019 11:36:49New subject after splitting |
|
9/9/2019 11:40 AM | |
Joined: 6/19/2017 Last visit: 4/19/2024 Posts: 7957 Rating: (162) |
Closed cause question posted twice.
Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on