1/16/2020 1:25 PM | |
Posts: 1 Rating: (0) |
I have the same problem with Minas A5II and I am trying to do a position control. I have already wired the Servo-On, NOT and POT to 0V. I can run motor with pulse train and NPN plc by using OPC1, PULS2 & SIGN2. Now, I want to use it with s7-1212C. How shall I wire it? I was thinking of using PULS1, PULS2, SIGN1 & SIGN2 with 2k ohms resistors. Like this: PLC 2 pulse generating terminals-> 2k resistors-> PULS1 & SIGN1 PULS2 and SIGN2 back to 0V. Will it work or is the Panasonic drives only for sink output? Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Shiroe at: 01/16/2020 13:26:24Last edited by: The Helping Hand at: 01/16/2020 18:02:44New subject after splitting |
|
Follow us on