12/19/2016 1:10 PM | |
Posts: 64 Rating: (2) |
Hi experts and all friends. I have read almost all modbus topics and I saw the benefit of topics that you have shared. Thanks. I have a project that needs modbus rtu with s7-1200 OLC. I have done with PLC. It is slave and I got another PLC for master and I have tested with master PLC my slave PLC-s7-1200 cm1241 is working without problem. My problem is that PC software can't comminicate with my PLC. I don't know where I do mistake. I have tried many softwares. One of them is Radzio.(http://en.radzio.dxp.pl/modbus-master- simulator/) but I don't know what my mistake is. What I have done is below; PC side On PC side 5611 comminication card is cabled as profibus cable. Radzio software (I have added a picture.) PLC side S7-1200-Slave (211-1AE40) (I have tested with other PLC which master) Both side I am sure Bitrare 9600 kb Parity none stop bit 1 Please I need to learn how to use PC as master because I can't find any PLC for master to test when I go to service for start-up the project. up the project. I also have attached a video. (https://youtu.be/Wmwo85S-2uM) |
12/19/2016 1:22 PM | |
Joined: 2/27/2014 Last visit: 4/19/2024 Posts: 689 Rating: (199) |
Hello, Plz try with Modview or modscan as Modbus Simulator software. I always test with this software and works fine without any issue. As Modview you can define as Modbus Master or slave as per your requirement. Use serial converter as RS485 to USB to check communication between PLC and PC. Just change the extension of ModBusView.txt to ModBusView.exe. AttachmentModbusView.zip (159 Downloads) |
With Best Regards, |
|
This contribution was helpful to2 thankful Users |
12/19/2016 1:54 PM | |
Posts: 64 Rating: (2) |
Duris_I I am using RS-485/422 two wire, I tested with another PLC on profibus cable |
12/19/2016 2:38 PM | |
Posts: 64 Rating: (2) |
DJ_1 I have tried to use your software but still same problem "timeout":-( |
12/19/2016 2:41 PM | |
Posts: 64 Rating: (2) |
Duris I am using the converter cable (http://www.s-link.com.tr/urunler/s-link-sl-32t-usb-to-rs232-cevirici-vaiec/) Is it correct cable that I am using? |
Follow us on