5/9/2019 8:18 AM | |
Posts: 11 Rating: (0) |
After many checks, I realized that: - Mismatch firmware is not a problem because I can connect to Azure Iot Hub via port 8883. - Proxy is also not a problem because It throw 80E4 error regardless I connect by company network or home network. - Installing new Broker support all TLS versions but error still happen. - Broker CA is x509 v3, and of course, Time of Day, CPU's Time, certificate ID are correct. 80E4 error still happen and I can't find any abnormal. Attached file is some my PLC configurations. Please, Could someone let me know what should i do now to correct it? Thanks a lot. AttachmentMQTT_Configure_80E4 error.pdf (309 Downloads) |
Last edited by: Noenoe at: 05/09/2019 08:47:36Last edited by: Noenoe at: 05/09/2019 16:27:24 |
|
5/10/2019 4:31 AM | |
Posts: 11 Rating: (0) |
Help me please!!! |
2/17/2020 11:48 AM | |
Joined: 10/28/2009 Last visit: 5/29/2023 Posts: 5 Rating: (0) |
Same problem me too... Any suggestion ? |
11/19/2020 2:20 AM | |
Joined: 12/18/2017 Last visit: 4/6/2024 Posts: 6 Rating: (1) |
Thanks to this post I was able to get the PLC talking to VerneMQ over TLS. I've done some packet sniffing on the S7-1200's TLS handshake and for everyone's benefit here's what I found: 1. gmt_unix_time is out of whack as of firmware 4.4.1 I have not verified if this value is generated by PRNG or is derived from actual time. However, it should be noted that most modern TLS servers will disregard this value and it should not cause any connection issues (letter in defense of removing gmt_unix_time: https://tools.ietf.org/id/draft-mathewson-no-gmtunixtime-00.txt) 2. TLS version: 1.2 only 3. Supported cipher suites:
4. Signature hash algorithms:
5. ECC Group: secp256r1 (0x0017) 6. ECC Point formats:
Hope these helps for those configuring their secure MQTT broker! |
Last edited by: Roy Chai at: 11/19/2020 02:24:47 |
|
Follow us on