10/18/2019 8:30 PM | |
Posts: 1 Rating: (0) |
Hello, I am also working with a 1215C CPU and a UR3e robot. I have a working profinet communication link set up, but there are specific commands that I need to send via TCP. I can not get the TSEND_C do do what I want it to. I have used a PC, running socket test, to test the settings and everything works that way. with connection false, status is 7000 with connection true, status is 7004 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/21/2019 08:25:47New subject after splitting |
|
10/21/2019 12:38 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12867 Rating: (1639) |
Hello Robert you can use this FAQ zo check if the Basics are correct: https://support.industry.siemens.com/cs/de/en/view/67196808 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on