10/15/2016 7:59 PM | |
Posts: 10 Rating: (1) |
Hello Experts I have come across this post while googling about libnodave library for S7 communication.
I am making my application in VB.NET language in Visio Studio 2012-Ultimate to read/write data between my PLC and my PC. I am able to add the "libnodave.net.dll". But I am not able to add "libnodave.dll" file to my VB project. I have attached screenshot of error message that pops out. I come with great expectation of guidance. Please help. By the way, I would really appriciate if someone could share any other alternate way out like some sort of alternate .NET codes to communicate with My S7200 Smart PLC. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/17/2016 12:32:38 PMNew subject after splitting |
|
10/16/2016 10:55 AM | |
Joined: 3/30/2011 Last visit: 9/18/2024 Posts: 736 Rating: (256) |
Sharp7 (C# Port of Snap7) |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
This contribution was helpful to1 thankful Users |
10/17/2016 5:27 AM | |
Joined: 3/14/2016 Last visit: 9/1/2024 Posts: 162 Rating: (45) |
Excuse me Sir, do you have a moment to talk about the open source Pascal SCADA? If it doesn't need to be in VB, off course. You'll be able to cross compile for Windows, Linux, ARM... Check the new website (being developed): And the project on sourceforge, feel free to join it if you want. |
"Engineers like to solve problems. If there are no problems handily available, they will create their own problems." (Scott Adams) |
|
8/12/2020 11:15 AM | |
Joined: 7/16/2019 Last visit: 9/17/2024 Posts: 1 Rating: (0) |
You need download libnodave.net.dll file at https://sourceforge.net/projects/libnodave/ to your PC and add references in the VB.NET project properties. |
Follow us on