7/5/2013 10:03 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi random222a, Try and make us know the result. |
7/10/2013 2:27 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi random222a, If I understand you want to backup the program? or what you want to do? |
7/10/2013 2:37 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello Press ESC + Up-Arrow during Power Up phase. For Detailed enstructions, pl see the Manual Extract attached. Hope this helps Cheers Navnag AttachmentOP27_OP37_Downlaod Mode.pdf (143 Downloads) |
There is no such thing as the last bug in a program |
|
7/10/2013 2:42 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi random222a, If I remember correctly you have to press the up arrow key and Escape key at the same time during startup of the panel. OP27, OP37 Operator Panels - Siemens Industry Online Support |
7/10/2013 6:43 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello random222a As suggested by Ste39,the best way to download program to OP37 is to use the RS232 port ( IF2 ). You will have to try different baud rates ( Start with 9600 )
You can also make the cable yourself ( Pl see the attachment for Pin Details ) You will need to use a USB to serial convertor if your PC does not have a serial port. Unfortunately these convertors are not always reliable. As you are testing the OP37,I would also suggest you look at Appendix C1 ( Hardware Tests ) in OP37 manual ( http://support.automation.siemens.com/WW/view/en/1142800) Hope this helps Cheers Navnag AttachmentCable_Details_PC_OP_RS232.pdf (96 Downloads) |
Last edited by: Navnag at: 7/10/2013 6:49 PMLast edited by: Navnag at: 7/10/2013 6:45 PMThere is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
7/11/2013 9:55 AM | |
Posts: 13 Rating: (0) |
Yes, IF2 and all other ports works, except IF1B, which is now my only target to connect. Colud I connect this IF1B directly to PC through any cable?
Thanks, I didn't know about these tests. Unfortunetly there is a problem again. I pressed that three arrows and keep pressed, but nothing happened, test mode didn't start (arrows keys are 100% functional). Why that could happened? I also checked this three arrows on other smaller OP27, and test mode opens instantly, so combination is good, but OP37 doesn't want react to them. |
Last edited by: random222a at: 7/11/2013 9:55 AM |
|
Follow us on