2/15/2019 7:05 PM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating:
|
Did you try and found tap not working? Or did you derive from the summary at http://cgit.openembedded.org/meta-openembedded/tree/meta-networking/recipes-support/openvpn/openvpn_2.4.6.bb?h=master#n1 that only tun is working with the package (I strongly suspect that this is not true). If we lack some kernel config, that is fixable (and can also be integrated into future releases). |
2/18/2019 6:50 PM | |
Posts: 7 Rating:
|
thanks Jan-K, as soon as i test it i will inform the topic |
This contribution was helpful to
1 thankful Users |
2/24/2019 10:24 PM | |
Posts: 7 Rating:
|
After many trials during weekend finally i succeed to build an image without any error. I worked with Vmware Debian image from osboxes.org *Debian 9.7 32bit and 64bit cannot produce image without error on the end. (.wic file not produced) Debian 9.6 64bit finally produce image without any error, only few warnings. (.wic file produced) After producing iot2000-example-image-iot2000.wic, i following the steps of CreateImageIOT2000_en.pdf and see that openvpn was already included because of layer meta-networking also all dependencies (openembedded-core, meta-python, meta-oe) bblayers.conf does not need to change at all because has already inside meta-networking. I changed only the iot2000-example-image.inc where i add the line IMAGE_INSTALL_append = " openvpn" I run again "kas build meta-iot2000/meta-iot2000-example/kas.yml" and i put the image to IOT2040. Althougt image working (node-red is ok) i don't see How can i adjust openvpn? Where i have to put my client .conf, .key, .crt files? |
This contribution was helpful to
1 thankful Users |
2/25/2019 7:40 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating:
|
Hi, you found the right way to build the image, nice If you run the kas script again without changing, the files (iot2000-example-image.inc and bblayers.conf) are used with its default values from github to build the image. So the added packages will not be included to the image. You either can change the kas script like described here in the last post OR use the bitbake command manually like described here at the end of the fourth post
Best regards! |
Last edited by: bergmanu at: 2/25/2019 7:41:46 AMNot working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on