6/30/2013 2:40 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hello friends, Please provide all tips related to editing the text messages in the forum that are not possible with the tools available here.Such trick as HTML code manipulation and other tricks you find out by experience.Some points may come from support but better to be shared with other members. While answering to the technical question, you may reach some points that you are not satisfied with the performance of text editor.For me the first solution is to ask the moderating team as they work with these tools everyday and also they access to developer of this forum.One of the most interesting topic I encountered this week was to create "Space In Enumeration". I was not happy with performance of editor in this posts, Have look. The texts are so close together and a space is really necessary between each option.After asking for support the following solution comes out:
The solution is easy and at the same time finding the right place to insert that code in HTML editor is not an easy job(see the attachment).For starting point, check the easiest case:
Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 6/30/2013 3:06 PMLast edited by: hdhosseini at: 6/30/2013 2:51 PM// typo |
|
This contribution was helpful to5 thankful Users |
6/30/2013 3:29 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477) |
Sometime its difficult when copying link above |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to2 thankful Users |
6/30/2013 5:18 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hello again, But I believe tricks are learned more effectively in practice like vocabulary ang grammar in use.I found and Online HTML editor here it did a great edition for me , change the font size and color of text at the same time.Sure can do more in practice without being involved in code manipulation.
Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 6/30/2013 5:19 PM |
|
6/30/2013 5:39 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477) |
Ok here is more easier way Just Open Word, type what you want, format it (change font size, Font type, color and all) and just copy and paste here Very easy… isn’t it?? |
Last edited by: Vithani at: 6/30/2013 5:40 PMLast edited by: Vithani at: 6/30/2013 5:40 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to2 thankful Users |
6/30/2013 6:01 PM |
|
Posts: 8946 Rating: (999) |
Test test test test TESTESTESTGreat!And the typo – check is also done! |
6/30/2013 6:02 PM | |
Posts: 8946 Rating: (999) |
Test test test test TES TEST EST Great! And the typo – check is also done! |
6/30/2013 10:24 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Thank you friends for nice and enthusiastic contribution, I just summarize what are our common points after all:
Best regards Hamid Hosseini |
This contribution was helpful to1 thankful Users |
Follow us on