7/13/2020 11:22 PM | |
Joined: 10/11/2019 Last visit: 8/25/2023 Posts: 27 Rating: (0) |
Hello! I'm trying to connect the PLCSIM Advanced as a OPC UA Client to a PC based OPC UA Server, but I'm unable to do that and I don't know why exactly. I noticed that the 'Status' output from all OPC_UA blocks have the same error message, 16#0070_0000 . Here is what I did so far: Under the OPC UA Communication folder: - Added a new interface with the server's configuration, such as IP address, no security, Read and Write lists; Here I was able to connect to the server and add the Read and Write list by simply dragging and dropping them into the OPC UA Client interface. Under the Program Blocks folder: - Added the OPC_UA Connect block for the connection, OPC_UA_NamespaceGetIndexList, OPC_UA_NodeGetHadleList and OPC_UA_ReadList. I was searching for some clearence here at the forum and noticed that some people had the same problem, but couldn't find the solution. Has anyone managed to connect to a PC Based OPC Server? I'm running TIA Portal 15.1 and PLCSIM Advanced 2.0 SP1 The project's archive is attached. I hope someone could help me! Thanks in advance! AttachmentAlex_OPCUA.zip (124 Downloads) |
Follow us on