3/21/2017 12:43 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello Jiri, Have you already seen this: S7 Communication with BSEND/BRECEIVE via PROFIBUS CPs - ID ... Try to open the project and look how is connected there is also a project to Exchange data, for FDL i will investigate, if I'll find something i'll let you know |
3/21/2017 12:55 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, info about FDL FDL Programming Interface - Siemens Support How do you program the communication blocks ... - Siemens Support |
3/21/2017 1:05 PM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating: (14) |
Hello Ste39, Thank you for the link - this is very interesting, how to transfer larger amount of data - but still it is S7 connection (BSend/BReceive via CPs). Thank you. Regards, Jiri |
Georgio |
|
3/21/2017 1:09 PM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating: (14) |
Hello Ste39, I can see FDL in the table for my CP. Please see attached picture. There is no particular information about number of connections, I hope that it is possible to have them more than 1 connections.. Thank you. Regards, Jiri |
Georgio |
|
3/21/2017 6:16 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, I don't think that you can to have more than 1 connection with 1 CP eg. 1 CP=1 connection. You should find the method of moving the data block to have two separate blocks eg. the first 236 bytes and another (I do not know what is missing to you) and call the first one then the other, and back to the first, you can surely, but I do not have ever done. |
Follow us on