12/15/2017 8:20 AM | |
Posts: 23 Rating: (0) |
Dear all, Probably for You it is simple problem. On customer site there are control cabinets with PLCs, HMIs, VFDs all in profinet. The problem is, the automation network is together with office subnetwork. Whenever there is a crash on office network also the profinet subnetwork is giving faults of higher level connection problem accress one local cabinet. You can see on drawing 1 what I mean. My idea is to add router (os something else) add give it another sub addressses on every cabinet, but still need to have connection with VPN and Scada to all. The disadvantage is that I do not have access to server computer and need to ask ITs. Can You advice me if it solve the issues with network crash? How to configure router so it forwards me to the local address? best regards AttachmentDrawing.zip (69 Downloads) |
12/15/2017 11:52 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, here you find a overview which CP and PLC support S7 Routing |
Follow us on