4/30/2019 5:05 AM | |
Posts: 7 Rating: (0) |
Good Day, we we're trying to re-assign IP address for IE/PB LINK PN IO device. we tried to use Primary setup tool and Simatic Manager (free trial version). However, it's not working. Hope you could help us. Thanks and Best Regards, Tolitz ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/30/2019 12:29:29New subject after splitting |
|
4/30/2019 12:35 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, ist the IE/PB Link found in Simtaic Manager oder PST Tool? Christoph |
4/30/2019 3:14 PM | |
Posts: 7 Rating: (0) |
Good Day, we cannot see it in the simatic manager and pst. we haven't try with Proneta. Thanks and Best Regards, Talawan, Rowelito S. |
4/30/2019 3:53 PM | |
Posts: 7 Rating: (0) |
No, we use it with power on. the default of the IE/PB Link PN IO light is same as the device new and start up. |
4/30/2019 3:55 PM | |
Posts: 7 Rating: (0) |
By the way, I also installed ProNeta. though, we do not have GSD file IE/PB Link PN IO. I hope you could help us. |
5/2/2019 6:09 AM | |
Posts: 7 Rating: (0) |
Good Day, Is it possible that there's no MAC address installed in the Gateway device: Thanks and Best Regards, Talawan, Rowelito S. |
Follow us on