4/13/2016 12:55 PM | |
Posts: 17 Rating: (0) |
HELLO please i want to read data from diris D50 , my connection is with the diris D50 and s7 1200 via Ethernet. i used the block MB.client to read data from diris D50 and i cannot i dont know why connect-id : 1 ip-1: 192 ip-2: 168 ip-3: 0 ip-4: 5 ip-port:502 mb-mode:0 mb-data-addr:40002 mb-data-len:10 mb-data-ptr: p#DB2.DBX0.0 REAL 100 here the table of diris d50 PLEASE HELP ME ! ------------------------------------------------------------------------------------------ |
Last edited by: Blue Moderator at: 4/13/2016 1:01:31 PMNew subject after splitting |
|
4/14/2016 11:04 AM | |
Posts: 17 Rating: (0) |
I HAVE CHANGED A LOT OF THING BUT I GET NO VALUE ! I WANT TO READ THE VALUE 18458 OF THE CURRENT BUT NO SOLUTION |
4/14/2016 11:05 AM | |
Posts: 17 Rating: (0) |
THE DB2 sturcture |
4/14/2016 11:06 AM | |
Posts: 17 Rating: (0) |
i have change the mb-unit-id even i dont know the right one cause i dont have this unit-id in the manual |
4/14/2016 11:08 AM | |
Posts: 17 Rating: (0) |
i have changed the parametrs of the mb-client but no results yet |
4/14/2016 12:52 PM | |
Posts: 17 Rating: (0) |
status =0 now i can read this data (ADD 18458). , i wonder if i can read all this data from what i will start ? THANK FOR THE HELP |
4/15/2016 10:06 AM | |
Posts: 17 Rating: (0) |
status once =8384 and no error , i will try to switch on/off the plc and i will tell you thank you so much |
4/15/2016 10:37 AM |
|
Posts: 17 Rating: (0) |
i dont understant your question ! please can you more explain |
4/15/2016 10:41 AM | |
Posts: 17 Rating: (0) |
last day i did the same thing and i succeded with no error and no status i try with the same parametrs but no resultat yet |
4/15/2016 10:43 AM | |
Posts: 17 Rating: (0) |
the mb-unit-id =17 in dicimal it means 11 in hexa |
4/18/2016 9:11 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Hello, any news? Check also this site where are helpfull applications to test better your connection: http://www.simplymodbus.ca/index.html Also some know-how is there, so look at this and make some tests from your PC to Diris for first. Give info pls. Update: applications can run without licensing, but f.ex. only 3 requests after each, then you must close application and run again. I got it tested on Win7 x64 without problems (still only RTU), but can be helpfull. Pls don't forget change application properties as WinXP SP3 compatible, this is clue for good functionality under Win7 x64. |
Last edited by: Duris_I at: 4/18/2016 9:16:36 AMWith best regards... |
|
4/18/2016 11:16 AM | |
Posts: 17 Rating: (0) |
DURID-I I tested with simplyModbus but there is no result yet i wonder if i have problem of Id of Diris d50 or address . |
Follow us on