2/8/2012 1:34 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24) |
Dear Primo, some comments regarding the documentation...
I agree with you that is a failure in the documentation! It is the TC_CON not TC_SEND. But the Parameter CONNECT is right. Of course you cannot set there 16#FEEDDADA directly but at the Parameter in the DB where the CONNECT is pointing to. E.g.: TC_CON --> CONNECT --> DB_xxxx (you have to create it, notice choseno optimized block access) --> param_xxxx (this is a variable you have to creat ewith DATATYPE "TCON_WDC") --> RemoteWdcAddress --> HERE YOU ENTER 16#FEEDDADA
Thats up to you, but did you understand the restriction regarding (this point is correct in the documentation :-) ) Regards |
Follow us on