6/8/2010 9:22 PM | |
Posts: 11 Rating: (0) |
I have a project which I'm looking at which requires a medium quantity of I/O at a number of different locations. The Master PLC (S7-1200 plus modules and local HMI) is located some distance from the distributed I/O and remote HMI displaying a mimic control of the system. I would like to use a Balluff BNI I/O module at each of the locations rather than using another PLC just for remote I/O. Any advice would be apprieciated.
Attachment869880_IndusNet_03_0911_en.pdf (557 Downloads) |
Last edited by: alanled at: 6/8/2010 9:24 PM |
|
6/9/2010 8:52 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Dear alanled, At this moment it is not possible to use S7-1200 in combination with Profinet See this link: With which devices can the S7-1200 communicate via the PN connection? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
6/9/2010 9:11 AM | |
Posts: 11 Rating: (0) |
So what you are telling me is I will have to use another PLC just for distribution. |
1/12/2014 1:55 PM | |
Joined: 3/20/2013 Last visit: 3/20/2024 Posts: 3 Rating: (0) |
Hi everybody, I tried the communications with S7-1200 and balluff io-link modules without any problem. It;s working very well. I attached file with my set with balluff profinet master and another io-link modul. I can’t see any problem also with the older versions of S7-1200 plc. Attachmentballuff io link.zip (604 Downloads) |
This contribution was helpful to1 thankful Users |
3/16/2015 3:32 PM | |
Joined: 5/28/2013 Last visit: 2/1/2023 Posts: 112 Rating: (3) |
What you mean? I made an entire Profinet network with 3 PLCs S7-1200, 3 ET-200S Remote I/O and 11 inverters G120C... |
6/1/2018 1:36 PM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7959 Rating: (162) |
New question published by Gustavo_Orige is split to a separate thread with the subject Integration of a 1214FC CPU with a BNI PNT-508 Balluff. Best regards |
Last edited by: Jen_Moderator at: 6/1/2018 1:39:15 PMEdited subject. My Forum is the place to personalize your profile, |
|
Follow us on