7/20/2011 8:52 AM | |
Joined: 4/24/2006 Last visit: 9/19/2024 Posts: 8739 Rating: (1168) |
Dear santy, You can only use the A solution in this faq: Ethernet Communication: Data Exchange between S7-1200 and S7-300/400 (CE-X18) But it is not possible using CP343-1 Lean. You will need CP343-1 Perhaps this thread might help: /tf/WW/en/Posts/56480 Best regards, Wizard |
Last edited by: Wizard at: 7/20/2011 8:55 AMWhen you use TIA portal v11 and S7-1200 cpu v2, you can use Put and Get from S7-1200. (S7-300 is server, so you can use CP343-1 Lean) |
|
7/20/2011 9:26 AM | |
Posts: 947 Rating: (45) |
Hi santy As variant: you can use profibus-slave module for 1200 and use master (315-2DP)-slave(1200). Or use profibus-master module for 1200 and use master (1200)-slave(315-2Dp) |
7/20/2011 1:54 PM | |
Joined: 4/24/2006 Last visit: 9/19/2024 Posts: 8739 Rating: (1168) |
Dear santy, When you want to use Profibus. And the S7-315-2DP is master, then you need the CP1242-5 (Profibus slave communication module)for S7-1200 Here you can download the GSD file, you can import in Step 7 V5.5: Download GSD File CM 1242-5 Best regards, Wizard |
Follow us on