3/27/2014 1:09 PM | |
Posts: 3 Rating: (0) |
Hello, I have a problem with FB block for sending UDP packets. It is possible for the SIMATIC S7-1200 to send a UDP packet as a broadcast packet? I used TUSEND, but I not posted nothing. You can do some simple example? Here is my test program. But I do not know why it does not work. Thank you ... AttachmentTEST.zip (705 Downloads) |
Last edited by: CS Moderator at: 4/1/2014 12:25 AMnew subject after splitting from /tf/WW/en/Posts/46768#top |
|
This contribution was helpful to1 thankful Users |
4/1/2014 3:44 PM | |
Posts: 3 Rating: (0) |
Hello... Much as I can understand... When I want to send a UDP or TCP packet, you must use the first function - TCON? And then, for udp - TUSEND and tcp - TESEND? |
4/3/2014 8:03 AM | |
Posts: 3 Rating: (0) |
Hello, This is not true. If you do upgrade Simatic S7-1200 to version 2.x, so it supports. |
4/3/2014 11:56 AM | |
Posts: 1368 Rating: (126) |
i also mean open communication... look at the picture in the attachment. Greetings |
4/3/2014 2:46 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (150) |
View of TCON call |
5/8/2014 3:45 AM | |
Posts: 10 Rating: (0) |
can you give us a sample on udp send and reseive datas? thank you so much |
5/8/2014 8:16 AM | |
Posts: 1368 Rating: (126) |
Hello Marko, so you build up a UDP connection successfully or with errors? Thanks for the feedback |
5/8/2014 8:19 AM | |
Posts: 1368 Rating: (126) |
Hello happydonkey, just have a look here http://support.automation.siemens.com/WW/view/en/29738463 http://support.automation.siemens.com/WW/view/en/38051505 http://support.automation.siemens.com/WW/view/en/91696622 |
5/8/2014 8:36 AM | |
Posts: 10 Rating: (0) |
the same question happens to me. have you got a good way to solve it? |
5/8/2014 8:47 AM | |
Posts: 1368 Rating: (126) |
Hello happydonkey, what exactly is your problem? Can you post more details or/and screenshots? Thx |
Follow us on