5/30/2012 12:05 PM | |
Joined: 8/31/2010 Last visit: 4/14/2024 Posts: 1509 Rating: (222) |
Hello laurensvl, Check this - Functions of the TS Adapter IE Basic(Sending e-mail) Other useful infor |
Like it? Rate it! |
|
5/31/2012 8:43 AM | |
Posts: 17 Rating: (0) |
Well I think it will be best to but a new cp because it seems the TS cannot deliver the correct functions for us. Thanks anyway for the help |
5/31/2012 11:07 AM | |
Joined: 8/31/2010 Last visit: 4/14/2024 Posts: 1509 Rating: (222) |
Hello laurensvl, If you are using CP 1242-7 then it can be used for TeleService also along with TeleControl application. Applications of CP 1242-7 |
Like it? Rate it! |
|
5/31/2012 5:51 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24) |
Hey,... maybe the technical support means something like an MAIL to SMS gateway? (http://en.wikipedia.org/wiki/List_of_SMS_gateways) However now you are using CP1242-7... Yes you have to create an own DB with that SDT "TCON-Phone" as datatype. then you have to parameterize it. note that you cannot change destination-phonenumber during a connection is established. you have to make discon and con again. note that the source phonenumber of received messages in the cpis not available in the plc. |
6/1/2012 9:31 AM | |
Joined: 8/31/2010 Last visit: 4/14/2024 Posts: 1509 Rating: (222) |
More info available here - SIMATIC NET S7-1200 - Telecontrol CP 1242-7 Operating Instructions |
Like it? Rate it! |
|
Follow us on