9/10/2012 2:56 PM | |
Joined: 9/27/2006 Last visit: 5/6/2024 Posts: 12257 Rating: (2666) |
Hello cheichaa; What type of connection are you trying to setup between your CPU and the Schneider HMI? Is this a Magelis panel? I know they generally support Modbus/TCP, if not what other comm. links does your panelsupport? If you look at chapters 10 and 12 of the ffollowing manual, you will see that the s7-1200 CPUs support Profinet natively, and through different communication modules/boards they also communicate as Profibus-DP master or slave, Modbus RTU (with a PtP pprocessor) or Modbus/TCP. SIMATIC S7 S7-1200 Programmable controller So basically you will have to find a common protocol between the CPU and the HMi and work from there. Hope this helps, Daniel Chartier |
9/10/2012 5:55 PM | |
Posts: 20 Rating: (0) |
This is the manual of the HMI and also im using s7-1200 .and i insalled on the HMI a support package for s7-1200 ( bought it from schneider)
AttachmentMagelis_XBTGT_XBTGT5430.pdf (627 Downloads) |
9/10/2012 6:56 PM | |
Posts: 20 Rating: (0) |
http://www.global-download.schneider-electric.com/8525797C002E49F6/all/E186401D7ACA803D852579FE005BBF93/$File/vijeo_designer_v6.1_news.pdf this is what i bought
|
Follow us on