7/16/2008 4:28 PM | |
Joined: 4/24/2006 Last visit: 5/3/2024 Posts: 8632 Rating: (1148) |
Dear vadvik, You should use FC11(PNIO_send) and FC12 (PNIO_recv) Have you seen this faq: http://support.automation.siemens.com/WW/view/en/26558253 Perhaps it's useful Best regards, Wizard |
7/17/2008 7:09 AM | |
Posts: 10 Rating: (0) |
Configuration net pro in the attached. |
7/17/2008 7:11 AM | |
Posts: 10 Rating: (0) |
Configuration slave plc with ms configuration in attached. |
7/17/2008 10:04 AM | |
Posts: 10 Rating: (0) |
Hello,
I arranged for slave configuration controller, through a virtual entrance-exit in the hardware configuration MS configuration. The master controller trying to take these exit sign with the functions FC11 (PNIO-SEND) and FC12 (PNIO-RECV) I do not get nothing. Functions fails 8184H System error or illegal parameter type. What I did not correctly? Sample my project in attachment! Best regards Vadvik AttachmentSample.zip (302 Downloads) |
7/17/2008 12:44 PM | |
Posts: 5822 Rating: (411)
|
Hello, well... may you explain why you want to start your I/O Data in your PLC at Byte 103 or Byte 104? I changed this to 0 and I also changed the Receive buffer length to 2 Bytes, as you selected it in your Project. By the way... as I do not know where the OP is connected to I left the networking... personally I would split it to the DP Port on the Master and the DP Network on the IWLAN/PB Link. J_Bell AttachmentSample_2.zip (366 Downloads) |
Follow us on