8/21/2020 9:33 AM | |
Posts: 1 Rating: (0) |
In our drive we have two interfaces 1. Profinet interface with two ports 2. Non profinet interface with one port Toplogy view doesn't show the second interface (non-profinet) when analyzing on network adapter connected with profinet interface. Attached in 'ProfinetInterface_PronetaBugReport.zip'. Whereas If I do analysis with non profinet interface (with "Include devices which do not support PROFINET" check box) I can only see the non profinet ports. Attached the PRONETA log as 'NonProfinetInterface_PronetaBugReport.zip' As far as snmp walk the mibs seems to be good. I like to know, What change shall be made in MIB to make the both interface visible in PRONETA? AttachmentProfinetInterface_PronetaBugReport.zip (38 Downloads) |
Last edited by: vkdinar at: 08/21/2020 09:34:35 |
|
Follow us on