6/1/2013 10:05 AM | |
Joined: 8/31/2010 Last visit: 9/20/2024 Posts: 1521 Rating: (227) |
Hello Larry, S7-300 does not support Ethernet/IP. TCON, TSEND, TRCV is typically used for TCP communication. Hardware catalog contains devices which are supported by the software itself or the devices for which the GSD / GSDML are installed. So typically for TCP communication you need not drag and drop any device to your Network view, proper configuration will do. For having a better idea on TCP communication you can go through this - How do you program the TSEND_C and TRCV_C instructions for open user communication over the integrated PROFINET interface of the S7-1200 CPU?- an example in TIA Portal but with S7-1200 How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300 or S7-400 CPU?- an example in S7-300 but in Classic software Anyhow the S7-300 TCP comm in TIA Portal will be more or less similar to the above mentioned S7-1200 example |
Like it? Rate it! |
|
9/2/2019 6:43 AM | |
Joined: 3/20/2019 Last visit: 6/9/2020 Posts: 1 Rating: (0) |
HI SIR, Please send us your scl program sample for my reference in system integration thank you. |
Follow us on