9/25/2019 9:03 AM | |
Joined: 4/14/2017 Last visit: 8/2/2023 Posts: 32 Rating: (0) |
Dear All, I have ABB VFD ACS550 with RETA 02 CARD, its communicating through S71500 over profinet. Its getting on off command and giving feed back to plc. The only problems is that VFD is not following the speed ref from plc. I can see the value given from plc as speed ref on vfd panel upper right corner(Pic "a") but vfd not following this reference. when I start vfd locally then its run ok but from remotely its not following speed reference given. ------------------------------------------------------------------------------------------ Attachmentpicss.zip (24 Downloads) |
Last edited by: The Helping Hand at: 09/25/2019 10:36:13New subject after splitting |
|
9/25/2019 10:37 AM | |
Joined: 8/21/2014 Last visit: 5/14/2024 Posts: 954 Rating: (13) |
Closed cause question posted twice. Second thread: ABB VFD ACS550 with RETA 02 CARD, communicating through S71500 over profinet: vfd not following reference Best regard, HH |
My Forum is the place to personalize your profile, |
|
Follow us on