4/30/2020 4:13 PM | |
Joined: 10/25/2016 Last visit: 1/25/2024 Posts: 4 Rating: (0) |
Hi, I have the same problem a yj0011. I create a Server on Node-Red with its endpoint. I can explore it from a PC based Client (UA Expert) but I can't connect to it via S7 1500 as client. When I create a Client Interface in TIA Portal and I create a new Read List, I can connect online to the server and extract the variables I want to read. The problem is that when I try to execute OPC_UA_Connect it doesn´t connect. When I activate REQ inpunt it goes Busy with 0070_0020 Status but afterwhile Busy goes off and Status goes 0070_000 but it doesn't activate Done output. I've tried writing the full path of tehe server (opc.tcp://192.168.0.100:55388/UA/... as I read in the 1500 Manual but still doesn't work. Has anyone have any idea about the problem? Thanks very much to all of you that makes those examples ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/04/2020 08:14:59New subject after splitting |
|
5/11/2020 10:20 AM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1645) |
Hello a general Example for OPC UA Client in S71500 is here: https://support.industry.siemens.com/cs/de/en/view/109762770 Do you have tested it first without Security? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on