11/30/2010 8:15 AM | |
Posts: 41 Rating: (0) |
Dear Sie, i have CPU 317-2PN/DP for Milling Section I have CPU 414-3PN/DP for Main Process Section I want to receive data from CPU 317-2PN/DP to CPU 414-3PN/DP over ethernet (Pofi net port). which instruction should i use to send & receive data to & fro? how should be the Hardware configuration( connections & setting in hardware & netpro) please post sample configuration & program is this case is only solved through Open communcation wizard or what is other method rahul Splitted from Open Communication Wizard Issues. Attachmentarchi.pdf (85 Downloads) |
Last edited by: O_Moderator at: 11/30/2010 9:13 AMnew subject after splitting |
|
11/30/2010 8:48 AM | |
Joined: 10/7/2005 Last visit: 5/13/2024 Posts: 3005 Rating: (1048)
|
Hello Raul0905 there areother methods and you can also use S7 communication (e.g GET/PUT, BSEND/BRECV and/or USEND/URECV) as well as Profinet I/O based data exchange. The CPU-CPU communication with SIMATIC controllers (compendium) has all the possible communciation ways listed in it and will hopefully come in handy now and in the future and below are a few selectedexample links: How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU? Sample program: S7 communication with the blocks SFB14 ("GET") and SFB15 ("PUT") with S7-400 Simatic Net Quickstart collection Once you decide on which way you want to implement the comms, it wont hurt to do a search for the relevant comms blocksas you may find more examples. I hope this helps |
Cheers |
|
Follow us on