12/11/2013 10:38 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
Hi, |
12/11/2013 10:49 AM | |
Joined: 1/5/2013 Last visit: 8/31/2024 Posts: 278 Rating: (16) |
yes |
12/11/2013 11:01 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
I guess this delivers the information you need and might be the only way to go: |
12/11/2013 11:27 AM | |
Joined: 1/5/2013 Last visit: 8/31/2024 Posts: 278 Rating: (16) |
Hi Owei, I'm asking in term of experience. Which is preferred at this case. |
12/11/2013 2:10 PM | |
Joined: 1/5/2013 Last visit: 8/31/2024 Posts: 278 Rating: (16) |
Thank you |
12/22/2013 2:10 PM | |
Joined: 1/5/2013 Last visit: 8/31/2024 Posts: 278 Rating: (16) |
Hi again, My network topology is attached. Which is better to use Telecontrol mode (with telecontrol basic server) or direct mode? since i don't have the devices yet, i'm in process by purchasing the hardware equipments and the required software. the communication will be ISO on TCP. in case of: 1- maximum number of remote stations that be connected to the central PLC using CP1242-7 with a- direct mode b- remote control mode 2- do the direct mode give the GSM signal strenth? Thanks AttachmentSCADA NW Topology v1.2 (SIEMENS Forum).pdf (131 Downloads) |
Follow us on