8/8/2019 8:48 AM | |
Joined: 8/3/2009 Last visit: 9/19/2024 Posts: 13742 Rating: (1730)
|
Hello first of all perhaps you mean V15 UPD3 not SP (there exists no SP3) -> you should check if you have set all your OS Stations with the Informations in the following Basic FAQ: https://support.industry.siemens.com/cs/de/en/view/108464289 Then check also: https://support.industry.siemens.com/cs/ww/en/view/88780011 Bye Murof |
If this Information really helps, you could use the Rate function |
|
8/8/2019 9:40 AM | |
Joined: 1/15/2018 Last visit: 7/26/2024 Posts: 18 Rating: (0) |
Thanks, yes I meant update 3! I have checked these. TWO of the four clients aren't connecting. One is giving Project Locked, the other is Server not available. BOTH have previously had the RT running successfully!
|
9/14/2019 11:51 PM | |
Posts: 1 Rating: (0) |
Conseguiu resolver o problema de ''project is blocked'' ? |
Follow us on