11/2/2007 11:53 PM | |
Posts: 5822 Rating: (412) |
Hello Ioana, well... you have two chances to add the SCALANCE X400 or X200 to the HW Config. 1. Way... Use them as PROFINET IO Device. If you have the latest versions of the X400, V 2.2.0, you can use the SCALANCE X also as Device GSDXML File... see for more information's also the Manual at: SIMATIC NET Industrial Ethernet Switches SCALANCE X-300 SCALANCE X-400 Configuration Manual 2. Way... Use them as SNMP units MIBII File. Than you can monitor the units with the SNMP OPC Server. Than you have to configure them in a PC Station with OPC Server and SNMP OPC Server. I hope I could give you some ideas. Best regards J_Bell |
Follow us on