11/13/2018 3:32 PM | |
Posts: 110 Rating: (0) |
no its just blinking .. |
11/13/2018 4:04 PM | |
Posts: 110 Rating: (0) |
I dont know what makes the problem.... :( |
11/15/2018 7:06 PM | |
Posts: 110 Rating: (0) |
Hi, How can i add CP343 v2.6 to HW catalog?? as siemens technical support saying its because of the version issue.. Regards Sandeep |
11/15/2018 9:10 PM | |
Joined: 4/17/2018 Last visit: 2/26/2024 Posts: 262 Rating: (60) |
Hello, This link can help you |
Last edited by: Jen_Moderator at: 11/16/2018 9:15:06 AMOptimized link. |
|
11/19/2018 9:17 AM | |
Posts: 110 Rating: (0) |
Hi Duris, Let me clear about the system. This is a cartooning machine which is having CPU314C-2DPC +CM321+FM350 counter module also there is 2 DP slave devices ie IM153 +Omron servo controller. As we need to monitor the machine in SCADA we just modified the HW config with CP343-1 module in the last slot.Then we saved compiled and downloaded the configuration and inserted the module.After Installing the module CPU goes to Stop mode with SF fault. If we remove the module everything is back to normal. But after 2days of normal operation we just inserted the module and now its working and the CP343-1 is able to ping. There is some bug for sure as after power off for 2-3 days it will show the same fault again Please find the attached original program without modification. Regards Sandeep AttachmentRB_Veet_.zip (108 Downloads) |
Follow us on