(3)| 1/5/2018 3:41 AM | |
|
Joined: 2/9/2016 Last visit: 10/28/2025 Posts: 83 Rating:
|
Dear All, i have a PLC-1200, HMI-TP-1200 & WINCC -7.4 . We need to generate a communication fault Alarm in Hmi & wincc if PLC is disconnected . ------------------------------------------------------------------------------------------ |
Last edited by: ANSHUMAN_SINGH at: 1/5/2018 3:43:35 AMLast edited by: CS Moderator at: 1/5/2018 11:15:27 AMNew subject after splitting Anshuman Singh |
|
| 8/6/2023 10:44 AM | |
|
Joined: 11/12/2020 Last visit: 4/29/2025 Posts: 11 Rating:
|
Correct me if I'm wrong, you want to create an alarm that indicates PLC connection status whether it is connected or disconnected, right ? If so, you can try WinCC System messages in Alarm logging editor. It has already-created messages for these purposes but they're not activated by default, find them and check their boxes to be used. For example, in winCC v7.4 sp1, these messages have the numbers 1000204 and 1000205 Check the help for the description of more system messages. |
| 7/2/2025 12:18 PM | |
|
Joined: 7/2/2025 Last visit: 12/11/2025 Posts: 5 Rating:
|
Dear Fabio 068, Can we do it using Ladder Logic
|
Follow us on